Hi Team,
My customer want to use the LM2623 for the boost from a super cap to 12V output.
As showed in the LM2623 datasheet, BOOT, VDD, EN and FB pins are not allowed to attached to the 12V, as the voltage of those pins must be below 10V.
I check the link which tell a reference design, which is suggested that the BOOT, VDD, EN and FB pins are connected to the input.
But my main concern comes from the super cap voltage, if it drops to 1V~1.2V, Can it still support the 12V output?
If considering the input of the voltage is 1.2V, how can we get the 12V output?
Expecting your response! Thanks!
https://e2e.ti.com/support/power-management/f/196/t/666808?tisearch=e2e-sitesearch&keymatch=LM2623