Hi,
We are intending to use BQ77915 for cell balancing and battery monitoring.
The queries regarding the IC are as follows:
1. Is VDIG regulator's output continuous or pulsed?
2. How can PACK- go to voltage less than VSS? In section 10.1.1.1 of the datasheet it is said that when gate of the CHG FET reaches ground, the PACK- will start to fall below ground. could you please elaborate?
3.What is the function of switch between output of VDIG regulator and VTB in the functional block diagram?
4. We are using 4 cell configuration of 4.2V each. When the battery pack voltage reaches about 14.5V while charging with a current of about 500mA, the CHG FET drive starts to toggle and if we decrease the charging current to about 80-100mA, the toggling stops. What may be the reason behind this?
Thank you
with regards
Yashaswini k