Hi Team,
Does the treset_filter apply to VIN as well as the FB input?
For example, if my input voltage spikes low (say to 3.3V) very quickly and crosses the UVLO threshold (which can be as high as 3.55V), but the Vreset threshold is not crossed (which can be as low as 3.03V -> 92% of 3.3V output), the device reset can be asserted, but if this event is fast enough, can it be filtered out by treset_filter?
Thank you,
Jared