Other Parts Discussed in Thread: OPA2209, , LM7705
I need to generate a very low noise negative voltage supply (below ground) for an opamp's V- power supply. The opamp (OPA2209/2210/2211) does not have rail-to-rail input and my input signal is expected to include (or come close to) ground, which is why I need the negative power supply. The supply must be low noise because the application is an analogue front end requiring ultralow noise performance.
I am considering the LM27762 charge pump which is advertised as low noise, but I am confused by the specifications in the datasheet, specifically "Output noise voltage" which is given as 22 µVRMS (IL = 80 mA, 10 Hz to 100 kHz), while the graphs for output voltage ripple have the ripple as anywhere between 0.75 and 3 mV (IOUT/VIN dependent). What are the differences between these numbers, which are orders of magnitude different?
Is there a better (lower noise, similar price and complexity) solution which I should be considering?