Hi Ti,
With the previous recommendation from previous thread that we need required the specs of Vin: 24V, Vout: +/- 12 Iout: 0.7mA. We have tested the split rail regulator design and found out the temperature of inductor increase rapidly when we draw 0.66A current from one side.
Test Methodology: A 5 ohm resistor is connected to the +3.3V power and Ground. The load draw about 0.66A.
The temperature hits 90 degree and continue increase until we turn OFF the power. In the calculator, we have calculated all the specs with ±1A, but currently the temperature don't allow us to draw current more than 0.66A.
Please help to advise.