Hi Team,
Here have one TPS549D22 peak current application question need your help for it.
The system load current application would be have two conditions as follows and need your help to see if it's okay with transient analysis.
Input 12Vdc, output: 0V9 normal
1. Load Current : Normal load 20A with 1msec period time then to peak current 100A with 25nsec period time and repeats
2. Load Current :Normal load 20A with 100usec period time then to peak current 100A with 25nsec period time and repeats
Best regards,
Albert Lee.