Hi Expert,
I ask 3 questions for TPS62813-Q1 operation.
Could you please support below items?
1,If the switching frequency is 1.8 to 3.5 MHz, is the inductor OK at 0.47 uH regardless of the load?
2,Is there an indication as to which setting from comp setting 1 to 3 should be selected at the start of design?
Although the output capacitor constant differs greatly between comp setting 1 to 3,
Does the output capacitor constant have to be changed significantly depending on the phase compensation?
3,Is it correct by the following calculation?
Comp setting 1
Rcf = 8.45 kΩ, fs = 18 ÷ 8.45 = 2.13 MHz
Best Regards,
Makimoto