Hi Team,
One of my customer requested for additional information on how the current limit is working for TPS2H160-Q1 and on below points.
1) During tests observed voltage of 0.78V when there is over current as well as when there is set limit current flowing and also in Open Load condition when no current is flowing through the load? How is this possible?
2) In Datasheet 8.3.6.1, it says that the MCU should turn off the switch in overload condition (highlighted in yellow). Can you clarify if the OUTx pins will go low by itself or will the MCU be required to make the output low? Right now, the statements are contradicting each other.
3) But in Table2 Fault table it is mentioned as in overload condition, the OUTx pins will go to low by itself.
Thanks in advance for the help and support.
Regards, Shinu Mathew.