Hi team,
i would like to konw why the min IN/OUT pins to Ground voltage is -0.3V in datasheet 6.1 Absolute Maximum Ratings.
Is it related to the internal protection circuirt? If so, can you share me a common circuit of Pin protection? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
i would like to konw why the min IN/OUT pins to Ground voltage is -0.3V in datasheet 6.1 Absolute Maximum Ratings.
Is it related to the internal protection circuirt? If so, can you share me a common circuit of Pin protection? Thanks.
Hello Hollis Liu,
Absolute minimum voltage on IN/OUT pins is -0.3V and this is due to the internal ESD protection circuit which has ESD diode from IN to GND. In fact all the LM5050 IC pins have this ESD protection and hence ESD diode from each pin to GND. These diodes are oriented with its anode connected to GND and cathode connected to IN or OUT or each other pins.
-0.3V is the forward voltage drop limit of the diode to limit its forward current. Also note that -0.3V is the rating across full operating temperature. Especially at -40C forward voltage limits drop to -0.3V, but at 25C it can handle -0.7V. Pushing these pins below, for a long time will damage the ESD diode and leads to pin short to GND.
Are you looking for reverse polarity protection on IN and OUT pins where these can handle large negative voltage below -0.3V?
Regards,
Kari.
Hello Hollis Liu,
If you need protection circuit to prevent IN/OUT pins from going below -0.3V, placing a shcottky diode from IN to GND and OUT to GND will prevent damage to the IC.
Regards,
Kari.