Hi,
I need to use TPS62801 at input voltage 1.8V typical +/-5% and VOUT=1.1V
TPS62801 is not able to have input voltage below 1.8V. I don't find any other reference.
What parameter is not guarantee at 1.7V input voltage ?
Thanks
Regards
Franck
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need to use TPS62801 at input voltage 1.8V typical +/-5% and VOUT=1.1V
TPS62801 is not able to have input voltage below 1.8V. I don't find any other reference.
What parameter is not guarantee at 1.7V input voltage ?
Thanks
Regards
Franck
Hi Franck,
The device is characterized and tested for the recommended condition in the datasheet. If the supply voltage is lower than the specification it will affect the performance of the device like load transient measurements, voltage drop, and others. I would suggest using the device within the range supply voltage specified in the datasheet.
Best regards,
Tanvee