Other Parts Discussed in Thread: TPS61196, , LP8556
I have attempted to modify a TPS61196EVM-600 to support two strings of 20mA LEDs but the TPS61196 does not appear to be starting up. I do not see any switching of the switching node and the Fault line is being driven low.
My LED strings are:
- Green, Qty 12, 3.2Vf, total Vf of 39.6V
- Blue, Qty 12, 3.3V, total Vf of 48V
I have modified my TPS61196EVM-600 with:
- Changed R26 to 240K to set current to 20mA
- Changed R23 to 160K to set head room to 200mV
- Changed R24 to 750K to set V(led_short) to 4V
Is there some other modification needed to allow the eval board to run with this LED setup? Thanks in advance for the help.