Other Parts Discussed in Thread: TL5001, LM5155
Hello,
A long time ago, I have done a regulation with TL5001A. My circuit :
Input comes from a 20Vac power supply and a rectifier. Thus V20 is about 28Vdc. C10 and C11 are discharged when main power is switched off (a 330R resistor is connected between V20 and ground when main AC power is lower than 3V for more than 1s). Thus, UVCO is reached after 3 or 4s without load. This discharge circuit is not on the schematic I have given.
Vout : 6.3V @ 10A (or 2.5V @10A with other feedback resistors).
When main power is switched on without any load, TL5001A will start as expected. With a 3A load also. But if I try to start this converter with, for example, an electronic load that consumes 5A, TL5001A doesn't start and Vscp raises to 2.4V. Converter detects a short circuit. If I pull SCP to ground, TL5001A starts as expected.
When TL5001A runs, I can raise output current until 15A without any trouble.
I have read "Circuit design calculations with TL5001" and I have tried to modify time constants (C2 and C3 in my case). If I modify C2 to 10µF, converter starts slower (I can show power on led) and stops with short circuit default. If I decrease C3 (I have tried until 12 nF), converter seems to start with greater load currents but with C3=47nF, efficiency falls (more than 3A/28V for 6.3V/4A !).
Second trouble. If main power supply is switched off and switch on again before UVCO condition is reached, TL5001A enters in protection mode also. I suppose these two issues are correlated but I haven't found solution.
I suppose I have done a mistake when I have computed R1, C3 and C2...
Help will be welcome.
Best regards,
JB