It is said that when changing the state of SET0 and SET1, there should be 500us delay. I tried pulsing them at the same time but i think the IC still functions correctly. Please give advice of what should i expect if there is no delay.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It is said that when changing the state of SET0 and SET1, there should be 500us delay. I tried pulsing them at the same time but i think the IC still functions correctly. Please give advice of what should i expect if there is no delay.
Hi James,
The 500us spec for SET0 and SET1 occurs when you need to switch back and forth between states. For example, on SET0, if you need to go from SET0=0 to SET0=1 then SET0=0 again, after you switch to SET0=1, you need to allow 500us to switch back to SET0=0. If you change SET0=0 to SET0=1 and also SET1=0 to SET1=1 for example, this should not be an issue doing instantaneously.
Thanks,
Abhinav.
I am confused. Based from datasheet, t_SET=500us is the delay between SET0 and SET1 pins.
From your explanation, it is different.
I tried the setup on the datasheet but even if there is no delay between SET0 and SET1 pins, IC seemed to be working well.
I have attached the details.SETx_Pins_Delay.docx
James,
While the datasheet says there is this minimum delay to transfer between the two pins, this is what is recommended. That being said, in your own testing, you might have found that this works with even no delay. This may work, but we do not guarantee it always switching in this case. If you wish to design with an instant swtich in mind, keep in mind that we don't officially support that configuration and if you have issues with the device not functioning correctly, it is due to this minimum Tset.
Thanks,
Abhinav.