Hi Sir,.
do TLVH431QDBVR claime in AEC-Q100 fileld ? thanks
do you share us the TI AEC products classify ?
thanks
Philip
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,.
do TLVH431QDBVR claime in AEC-Q100 fileld ? thanks
do you share us the TI AEC products classify ?
thanks
Philip
Hi PYTsai,
1. The TLVH431QDBVR is not AEC-Q100. This is device is rated from -40C to 125C but it is not AEC-Q100.
The datasheet in my first post has the TLVH431 that are AEC-Q100 qualified.
2. Yes the TLVH431QDBVR is a 1.5% device. This means its initial accuracy at 25C can be between 1.222V to 1.258V. The line below is the expected max deviation across temperature that include the initial accuracy.
If you want the accuracy across temperature, then it would be 1.194V to 1.286V which is a larger range than 25C due to temperature drift.