Hi, I need a buck converter for a board which has a VHF packet radio transceiver. I'm bucking from 14V to 5 V. The 5V feeds a 3.3V LDO which powers the transceiver.
The five volts also powers USB host, (500ma out), and is for this that I need the buck, otherwise I would have just used an LDO.
I have chosen TPS62147 because the data sheet says it has "very low output voltage ripple, minimizing interference with RF circuits." Also, most of the time, the board will only be drawing 10 to 20mA and the DCS
topology can slow down its frequency, maintaining efficiency, but most importantly reducing noise that may effect the radio.
Webench design has a 1.5uH inductor, but I thought a 2.2uH would be better because it has lower ripple (perhaps less RF noise as well or not??) The higher inductance means a higher frequency. At 10 mA this is a good thing as it means less ripple out, but at 500mA it means 800kHz instead of 600kHz which could make more EMI??
Do you think I would benefit from an input filter ?? If I use an input filter with Fo of 800kHz would it have deleterious effects on the buck converter as it moves to lower frequencies,?
Would It be beneficial to isolate the ground planes between the buck converter and RF module with a ferrite bead??
Thanks for taking the time to help me out.
Cheers
Matt.