Hello
Currently we are using the UCC27712 with a 12V power-supply and a highside mosfet with a 5V Vgs threshold-voltage.
We are driving the gate with the doubled voltage, which would actually be needed. We only need 5V Vgs, but the mosfet is driven with 12V Vgs, because the Cboot ist charged up on 12V.
Our mesurements show, that charging the gate far over the threshold-voltage causes some problematic switching-delays.
A great solution to this would be, not to charge Cboot up to 12V, instead limiting this volatge. Therefore we built in a z-diode between Rboot and Cboot and generated a voltage-drop form VDD to HB. This simply limits the voltage Vboot, which then drives the gate. Another solution would be, to build in a z-diode directly between the gate and the source of the mosfet. But this second solution is not prefered, because it increases the capacitance at the gate.
However, our prefered solution only works until we limit Vboot to 8V (Vz of the z-diode => 4.7V). When we increase the voltage-drop from VDD to HB further, the gate-driver stops driving the mosfet.
If I understood the datasheet correctly, then the uvlo of the UCC27712 is not the reason to this.
Why does this gate-driver stops switching, if Vboot ist limited this way? Would you recommend not to use the z-diode this way? Or is it unproblematic to generate a drop from VDD to HB?
With best regards
Eric Walser