Part Number: TPS68470
I am using TPS68470 in one of our design, i am not using Buck from this PMIC.
Any termination guidelines if Buck is not used. Specifically these G7 and H6 pins.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS68470
I am using TPS68470 in one of our design, i am not using Buck from this PMIC.
Any termination guidelines if Buck is not used. Specifically these G7 and H6 pins.
Hi,
Please ensure that Bit 0 (ENABLE field) of register 0x48 (VDCTL) is always set to 0 to disable the core buck regulator. This bit's default value on reset is 0.
When the buck is disabled:
Thanks,
Gerard
Hi Gerard,
Will there be any issue if Bit0 of register 0x48 is not set to 0? We are reusing FW between the design and hence the question.
Thanks
Mallari
Hi Mallari,
This bit disables the output of core buck regulator and powers down the internal control circuitry for this regulator. If this bit is not set to 0, the buck control circuit will turn on and attempt to regulate even if the converter is not connected or used in the application, resulting in unnecessary current consumption.
Thanks,
Gerard