This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

UCD9222: Firmware

Genius 9515 points

Replies: 2

Views: 85

Part Number: UCD9222

Customer ran into an issue with the UCD9222 where its firmware seemed to get corrupted.  They are trying to compare the checksum.  They can see the options for checking the checksum but they are all grayed out.  Also, they cannot find the devices when scanning in ROM mode, if they scan by device ID they are able to find the devices.

I've suggested connecting using these settings: https://e2e.ti.com/support/power-management/f/196/t/580624?UCD9222-Firmware-issue

Where can we find the firmware for these devices to see if we can update the firmware and get the device back working or if you could help to get the GUI working such that I can evaluate the checksum on these devices to see if it is corrupt?

Is the default firmware image included with Fusion Digital Power™?

Please advise.

Thanks,
Mark

  • Hi Mark, 

    The default firmware setting should be found in Fusion OFFLINE mode. 

    You can open Fusion OFFLINE mode, find UCD9244 and save the configuration to .xml file. 

    Then you can import the .xml file to the physical part. 

    Make sure to save the existing configuration in the part before you import default setting. 

    Thanks

    Qian

  • In reply to Qian Chen:

    Thanks Qian.

    Regards,
    Mark

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.