Hi,
We are using TPS65910A3 and have a question about the datasheet.
I'm looking at TPS65910A3 datasheet(SWCS046U) page.16
"5.7 I2C Interface and Control Signals".
I want to know max value of each parameter,
but it seems that "unit" are written in column of "Max".
Is it typo of the datasheet?
I checked the I2C specification documents and compared the value of
each parameter in the datasheet.
I guess that it is typo and the datasheet should be as follow:
If my guess is correct, when will the datasheet be update?
Could you tell us the schedule?
best regards,
g.f.