Hi, I implemented on a PCBA the typical application schematic found in the TPS54531 datasheet, as I need a power supply with equivalent specs. I am currently using it with a 14 V input. When the voltage on EN is higher than 1.25 V or when it is left floating, the device is having the expected behaviour and has a 5V output. When the EN voltage is below 1.25 V, 0 V in my case, I was expecting the output of the device to be off, but it is actually 5V. Even weirder, when a load is applied to the output, the voltage rapidly drops and when the load is removed the voltage goes back to 5V.
At the end of the day, what I am trying to do, is control the EN pin with a microcontroller to enable and disable the 5V supply. Is it theoretically possible? Do you see an issue?
Regards,
Leonard