Other Parts Discussed in Thread: LM5170
Dear support member,
Hi, I bought the model LM5170EVM-BIDIR. I want to make it operate as a buck converter.
Desired operating as below:
Input Voltage: 48V
Output : 12V and charge to battery
The set up is as the attached picture.
When I close J36 and do not used ISETA, the output voltage is 14.5V. How can I control the output current with this fixed voltage value? I want to charge a 12V battery with different current values. I mean I need a controllable output current but at fixed 12V or 14.5V.
When I open J36 and use ISETA (0 to 1.5V), the output voltage is kept at 20V. It's not possible to use the DC/DC converter to any application.
Can you give me some suggestions for my problem?
Thank you so much and I am looking forward to your response.
Best Regards,