hi
I have a new design with BQ27425-G2A and 3.7V lipo battery.
When I measure the resistance between SRX and VSS I get ~200Kohm ,
Once I connect the battery I get around 0.9V voltage difference between SRX and VSS.
When measuring the VCC pin I get 2.5V, which seems ok.
Can you suggest what may be the problem?
Is it worth mentioning that have the same problem in two differnet boards.