How can I adjust the system voltage of the buck. I just found the upper and lower limits in the datasheet but not how to adjust the system voltage it self. I would like to have a system voltage not higher than 3.6 volts.
Regards Raphael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How can I adjust the system voltage of the buck. I just found the upper and lower limits in the datasheet but not how to adjust the system voltage it self. I would like to have a system voltage not higher than 3.6 volts.
Regards Raphael
Raphael,
You can set the minimum system voltage when the battery is discharged using REG01b[0:3]. Default is 3.5V. However, after the battery charges higher than 3.5V, V(SYS) follows V(BAT) up to the battery regulation voltage + ~150mV. So, when the battery is fully charged, V(SYS)=4.2V+150mV = 4.35V. This is how all of our power path chargers function. If you need a lower system voltage, then I suggest adding a buck converter with 100% duty cycle following V(SYS).
Regards,
Jeff
Hi Raphael,
If using a LiFePO battery, I recommend that you start the charger with /CE pin = high, With /CE pin=high, the SYS output will initially regulate to MINSYS=3.6V. Then use I2C to change the VBATREG register = 3.6V and the MINSYS voltage register to something lower than 3.6V like 3.3V. The I2C settings will stay assuming you periodically write to the watchdog timer bit or disable watchdog timer, unless the charger is completely powered down. Then you can use your host GPIO to pull /CE pin low for LiFePo charging.
Regards,
Jeff