Hi Team,
My customer uses Chroma 6312 series E-load to test the TPS62085 EVM.
The configuration is listed below.
Vin=3V
Vout=1.2V
When setting E-load to CC mode at 2A, TPS62085 failed to build up the output voltage during booting on.
But if adding E-load after booting on, the output voltage is normal.
It's kind of you to look into this problem for us.
Thanks
Sincerely,
Edward