Hi Team,
My customer is planning on using our LM3881 to power the enable pin of the TPS22954. A concern of my customer is that the TPS22954 may turn on due to the Vflag votlage ramping up as it's input voltage ramps as well as seen in the table below for the LM3881.
The Vflag will be connected to the EN pin of the TPS22954 which has the below threshold voltage with min of 0.65V which is close to the VFLAG voltage spike.
It looks like the flag voltage does rise to 0.65V from that graph. Could you confirm that this is indeed the case? Also, what is the period of time that the voltage will be at or above 0.65V?
Thanks!
Best Regards,
Alfred