Other Parts Discussed in Thread: TPS65131
Hello,
Hi, I'm developing a circuit for guitar including an OPA1641 as pre-amp, and 2 buffer stages. My design will require +/-15V, generated from +9V (or 3.3-5V if required, those voltages will be available on the design too). In terms of power for those stages, the requirements are not completely defined yet, but they will be under 300mA.
I made a similar question at https://e2e.ti.com/support/audio/f/6/t/861629, and they made some recommendations and suggested to touch base in this forum.
I was considering to use the TPS65130 but they mentioned it could be too noisy for this audio application, and it would require further filtering, by a passive LC or by using a dual output LDO. Since space could represent another constraint (I mean, the extra filtering would require additional parts), could you please recommend an approach on this matter? Maybe some application note. We could also lower the split voltage to +-12V instead of +/-15V if that represents an issue, so maybe you can recommend a more appropriate converter.
Thanks!