Hi,
I have been facing a problem for the past one day. I have designed a circuit based on the Webench design tool. I followed the instructions of the tool to purchase the components as said.
My Requirement is :
V in = +5V
V out = -5V
I out = 200 mA (max) , Nominal (20mA)
Using this input, the circuit is created by tool. When I test it with real time circuit, output is only -1.4 V for +5V input. I am not sure what causes the problem. But when I check the flyig capacitor it is charged to 4.6V. Why this charge is not fully transferred to output capacitor C out ? What causes this problem? Help me out. Thank you!