Other Parts Discussed in Thread: BQ27Z561
I have a small battery-operated portable device for which I want to extend its use-time with an additional external battery. The two batteries are 3.7V LiPo of different size: The small battery is about 70mAh and the larger external one is about 280mAh (but could go as high as 1800mAh).
However, when unplugging or swapping the larger external battery, I want the device to stay "on" with the small internal battery still connected. I would then reconnect a freshly-charged larger external battery, or charge both in parallel when overall charge is low.
What would be my challenges for fuel-gauging and charging this 1S2P configuration with the BQ27Z561EVM-011?
Any recommendations for power path management or other issues?
Please let me know.
Thanks,
Carl Olen