Other Parts Discussed in Thread: LM2623,
Hi,
I am designing a battery powered board. My battery voltage drops to 1.6 V. So I wanted to use LM2623 Step-Up Converter (PCB draws 200mA@1.6V). I read LM2623' datasheet and LM2623EV's datasheet. On the LM2623EV's datasheet it is written that min input voltage is 2.3V but LM2623's datasheet says min input voltage is 0.8 V.
Which one shoul I consider ?
Best Regards