Other Parts Discussed in Thread: TPS2115A
Hello,
the TI costumer support told me to ask my question here.
At the moment I develop a new product and need some help with the power components to find the best solution. I have several ideas until now, but want I think there are better ways so solve my problem.
These are the facts:
- usb2 connection for 5V and data -> EMI components needed
- primary battery with 3x AA as alkaline or NiMh
- deep discharge protection for the battery needed, disconnecting from load, automatic reset if new batteries are inserted
- switch for selecting voltage source, batteries should not be charged, perhaps TPS2115A
- LDO for 3.3V (200-500 mA peak) needed
I hope these data are usefull and you can give me some hints which components are useful.
Best regards,
Jens