Other Parts Discussed in Thread: UCD90SEQ64EVM-650,
Hello,
I am using the UCD90SEQ64EVM-650 evaluation board with the 10-Rail Sequencer and System Health Monitor with 10-Fan Control and setting up the 10 fans in the Fusion Digital Power Designer GUI in the offline mode. When I try to assign the PWMs for a fan to PWM3 (pin 42 - PWM3/GPI3) or PWM4 (pin 41 - PWM4/GPI4), the GUI pops up with the Fatal Program Error copied below and shuts down the program.
The GUI is fine if I assign either of these pins to a fan Tach. line or as a GPI, but it won't let me assign them as PWMs even though the data sheet for UCD90910 and the Pin Selector in the GUI shows that these two pins can be used for fan PWMs. For reference, I would like these pins to both be set to 25KHz initially, which is within the frequency range for them, but I cannot get to the step to input the frequency because the program shuts down before I can add this.
Is there a bug in the GUI that is causing the Fatal Program Error when I try to assign fan PWMs to PWM3 and PWM4? Do I need to set something else up beforehand to use these two pins as PWMs?
Thank you.
Overview
--------
Application: Fusion Digital Power Designer 7.2.1.0
Operating System: Microsoft Windows NT 6.2.9200.0
.NET Runtime: 4.0.30319.42000
Memory Used: 125.00 MB
Exception
---------
System.ArgumentOutOfRangeException: Index was out of range. Must be non-negative and less than the size of the collection.
Parameter name: index
at System.ThrowHelper.ThrowArgumentOutOfRangeException(ExceptionArgument argument, ExceptionResource resource)
at TIDP.WinForms.Apps.DPGUI.el.au()
at TIDP.WinForms.Apps.DPGUI.el.a0()
at TIDP.WinForms.Apps.DPGUI.el.az(Object A_0, EventArgs A_1)
at System.EventHandler.Invoke(Object sender, EventArgs e)
at DevExpress.XtraEditors.Repository.RepositoryItemRadioGroup.RaiseSelectedIndexChanged()
at DevExpress.XtraEditors.RadioGroup.set_SelectedIndex(Int32 value)
at TIDP.WinForms.Apps.DPGUI.el.ar(Object A_0, a A_1)
at System.EventHandler`1.Invoke(Object sender, TEventArgs e)
at TIDP.PMBus.Parts.UCD90XX.Controls.b.a(h A_0, h A_1)
at TIDP.PMBus.Parts.UCD90XX.Controls.b.a(PinUse A_0)
at TIDP.PMBus.Parts.UCD90XX.Controls.b.a(Object A_0, OpenLinkEventArgs A_1)
at DevExpress.XtraEditors.Repository.RepositoryItemHyperLinkEdit.RaiseOpenLink(OpenLinkEventArgs e)
at DevExpress.XtraEditors.HyperLinkEdit.ShowBrowser(Object linkValue)
at DevExpress.XtraEditors.HyperLinkEdit.DoClick()
at DevExpress.XtraEditors.HyperLinkEdit.OnClick(EventArgs e)
at System.Windows.Forms.Control.WmMouseUp(Message& m, MouseButtons button, Int32 clicks)
at System.Windows.Forms.Control.WndProc(Message& m)
at DevExpress.Utils.Controls.ControlBase.WndProc(Message& m)
at DevExpress.XtraEditors.TextEdit.WndProc(Message& msg)
at System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m)
at System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m)
at System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)
Loaded Assemblies
-----------------
Accessibility
Version: 4.0.0.0
Info Version:
4.8.3752.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/Accessibility/v4.0_4.0.0.0__b03f5f7f11d50a3a/Accessibility.dll
Public Key Token: B03F5F7F11D50A3A
Com.Muegel.Misc
Version: 2.0.88.29979
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Com.Muegel.Misc.DLL
Public Key Token:
Com.Muegel.WindowsApp.Win32API
Version: 7.0.0.29979
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Com.Muegel.WindowsApp.Win32API.DLL
Public Key Token:
DevExpress.Data.v6.2
Version: 6.2.10.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.Data.v6.2.DLL
Public Key Token: 79868B8147B5EAE4
DevExpress.Utils.v6.2
Version: 6.2.10.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.Utils.v6.2.DLL
Public Key Token: 79868B8147B5EAE4
DevExpress.XtraBars.v6.2
Version: 6.2.10.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraBars.v6.2.DLL
Public Key Token: 79868B8147B5EAE4
DevExpress.XtraEditors.v6.2
Version: 6.2.10.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraEditors.v6.2.DLL
Public Key Token: 79868B8147B5EAE4
DevExpress.XtraGrid.v6.2
Version: 6.2.10.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraGrid.v6.2.DLL
Public Key Token: 79868B8147B5EAE4
DevExpress.XtraNavBar.v6.2
Version: 6.2.10.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraNavBar.v6.2.DLL
Public Key Token: 79868B8147B5EAE4
DevExpress.XtraPrinting.v6.2
Version: 6.2.10.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraPrinting.v6.2.DLL
Public Key Token: 79868B8147B5EAE4
DundasWinChart
Version: 7.1.0.1810
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DundasWinChart.DLL
Public Key Token: A4C03DCE5DB22406
Free.CommandLine
Version: 2.0.88.29979
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Free.CommandLine.DLL
Public Key Token:
Free.Misc
Version: 2.0.88.29979
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Free.Misc.DLL
Public Key Token:
Free.WinForms.Misc
Version: 2.0.88.29980
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Free.WinForms.Misc.DLL
Public Key Token:
Fusion Digital Power Designer
Version: 7.2.1.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Fusion Digital Power Designer.exe
Public Key Token:
Microsoft.GeneratedCode
Version: 1.0.0.0
Info Version:
<empty>
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
Public Key Token:
Microsoft.mshtml
Version: 7.0.3300.0
Info Version:
<empty>
Location: file:///C:/Windows/assembly/GAC/Microsoft.mshtml/7.0.3300.0__b03f5f7f11d50a3a/Microsoft.mshtml.dll
Public Key Token: B03F5F7F11D50A3A
Microsoft.VisualBasic
Version: 10.0.0.0
Info Version:
<empty>
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/Microsoft.VisualBasic/v4.0_10.0.0.0__b03f5f7f11d50a3a/Microsoft.VisualBasic.dll
Public Key Token: B03F5F7F11D50A3A
mscorlib
Version: 4.0.0.0
Info Version:
4.8.4121.0
Location: file:///C:/Windows/Microsoft.NET/Framework/v4.0.30319/mscorlib.dll
Public Key Token: B77A5C561934E089
System
Version: 4.0.0.0
Info Version:
4.8.4001.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
Public Key Token: B77A5C561934E089
System.Configuration
Version: 4.0.0.0
Info Version:
4.8.3752.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Configuration/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll
Public Key Token: B03F5F7F11D50A3A
System.Core
Version: 4.0.0.0
Info Version:
4.8.4121.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Core/v4.0_4.0.0.0__b77a5c561934e089/System.Core.dll
Public Key Token: B77A5C561934E089
System.Data
Version: 4.0.0.0
Info Version:
4.8.4121.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_32/System.Data/v4.0_4.0.0.0__b77a5c561934e089/System.Data.dll
Public Key Token: B77A5C561934E089
System.Data.DataSetExtensions
Version: 4.0.0.0
Info Version:
4.8.3752.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Data.DataSetExtensions/v4.0_4.0.0.0__b77a5c561934e089/System.Data.DataSetExtensions.dll
Public Key Token: B77A5C561934E089
System.Drawing
Version: 4.0.0.0
Info Version:
4.8.3752.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Drawing/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
Public Key Token: B03F5F7F11D50A3A
System.Numerics
Version: 4.0.0.0
Info Version:
4.8.3752.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Numerics/v4.0_4.0.0.0__b77a5c561934e089/System.Numerics.dll
Public Key Token: B77A5C561934E089
System.Web
Version: 4.0.0.0
Info Version:
4.8.4075.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_32/System.Web/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Web.dll
Public Key Token: B03F5F7F11D50A3A
System.Windows.Forms
Version: 4.0.0.0
Info Version:
4.8.4121.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms/v4.0_4.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
Public Key Token: B77A5C561934E089
System.Xml
Version: 4.0.0.0
Info Version:
4.8.3752.0
Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
Public Key Token: B77A5C561934E089
TIDP.DevEx.Skin1
Version: 1.0.0.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.DevEx.Skin1.DLL
Public Key Token: 95FC6C5621878F0A
TIDP.I2C.DeviceGUI
Version: 1.0.0.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.I2C.DeviceGUI.DLL
Public Key Token:
TIDP.Misc
Version: 7.0.0.20998
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.Misc.DLL
Public Key Token:
TIDP.Net.ProxyPrefs
Version: 1.4.0.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.Net.ProxyPrefs.DLL
Public Key Token:
TIDP.PMBus
Version: 7.0.0.42754
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.DLL
Public Key Token:
TIDP.PMBus.Design.TimeModel
Version: 2.0.88.20999
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.Design.TimeModel.DLL
Public Key Token:
TIDP.PMBus.DeviceGUI.UCD3000
Version: 7.0.0.42772
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.DeviceGUI.UCD3000.DLL
Public Key Token:
TIDP.PMBus.ParameterControls
Version: 7.0.0.42768
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.ParameterControls.DLL
Public Key Token:
TIDP.PMBus.WinForms
Version: 7.0.0.42771
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.WinForms.DLL
Public Key Token:
TIDP.SAA
Version: 2.0.88.20999
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.SAA.DLL
Public Key Token:
TIDP.SAA.WinForms.Misc
Version: 2.0.88.41447
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.SAA.WinForms.Misc.DLL
Public Key Token:
TIDP.WinForms.Apps.DPGUI
Version: 7.0.0.42773
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Apps.DPGUI.DLL
Public Key Token:
TIDP.WinForms.Apps.DPGUI.DPGUI1
Version: 7.0.0.1637
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Apps.DPGUI.DPGUI1.DLL
Public Key Token:
TIDP.WinForms.Apps.DPGUI.HelpCenter
Version: 7.0.0.41447
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Apps.DPGUI.HelpCenter.DLL
Public Key Token:
TIDP.WinForms.Dundas
Version: 2.0.88.21000
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Dundas.DLL
Public Key Token:
TIDP.WinForms.Misc
Version: 2.0.88.41446
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Misc.DLL
Public Key Token:
TIDP.WinForms.Util
Version: 2.0.88.20999
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Util.DLL
Public Key Token:
XtraDataTempAssembly
Version: 0.0.0.0
Info Version:
<empty>
Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.Data.v6.2.dll
Public Key Token: