This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 51
Part Number: ATL431
Hi Team,
I have a questions from a customer.
We are thinking to use this as a Zener replacement due to its accuracy on “tripping” point. For this we would need bit more information on the cathode leakage current when the Vref is not directly connected to the cathode. The datasheet Fig. 4. gives only information on the case where cathode and Vref are shorted.
Do you have cathode leakage current (Ika) measurement data available for the case where the cathode voltage is much higher (~10…11V) than Vref?
We would also need this for following temperatures -40, 25 and 85C in order to estimate the system reliability.
Would you be able to help with the requested data or pointing it out in the data sheet?
Thanks
Hi Alvaras,
I do not have this data on hand, but I can try to see if we have it internally. Can I ask what end equipment this is for?
Thanks,Abhinav.
If you think this response answered your questions/concerns, please click the button to let us know!