Part Number: LM5176
Other Parts Discussed in Thread: INA213, LMV431A
Dear *,
we are designing a Buck-Boost supply with LM5176 and want to limit input power to 25W. We will use ISNS at the input current.
Our input voltages in normal operation are from 12V to 24V, while UVLO=9V and Vhys=1V, for vin high we allow +3V
So the Vin range is from 9V to 27V. In-order to limit the input power to 25W, and if the RSNS is constant , then we have for different input voltages/currents different voltage drops across Rsns that will satisfy 25W.
Eg for 12V max input current is 2A and for 24V is 1A and so on. If we size the Rsns for lower voltages ( eg 12V 2A) then this will not work for 24V.
Is it possible to control the SS pin with a DAC in conjunction with ISNS input current in-order to limit input power to the LM5176?
Or is there a better way to limit input power of the LM5176?
Best Regards,
David.