Part Number: LM285-1.2
What occurs to the voltage reference under over current conditions? Does the device short, open or other? Up to 72mA may be seen under fault conditions.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM285-1.2
What occurs to the voltage reference under over current conditions? Does the device short, open or other? Up to 72mA may be seen under fault conditions.
First, thanks for responding.
Using an LM285. Did some testing on the parts. I thought (meant) to say what happens under over current conditions. Graphs show up to 30mA. Ran the test unit and had 250mA through it. Brought current back to norm and it still functions. I was looking for the temperature rise. Measured >170F. Tough part. impressed. Initial current under my conditions was 250mA then dropped to 220mA as the temperature increased. This is due to the Vref increasing.
Thanks,
Stan
Hi Stan,
This is interesting behavior. Before I received the devices to test it out on my side, our lab is closed due to covid19 precautions.
Can you share with me the schematic you are using?