Other Parts Discussed in Thread: BQ25713
Hello,
I am currently using the TPS51220 as a DCDC on my system, generating 12V and 5V from a 19.5V source. I am seeing issues once I start drawing current from the TPS51220. Below are three images to help explain my issue.
- Block diagram of the power path architecture for my system, highlighting connections for oscilloscope measurements
- Oscilloscope capture where V_BATT was supplied by the TPS51220
- Oscilloscope capture where V_BATT was supplied by an external bench supply
- Schematic for the TPS51220 on my design
As shown in the block diagram, the TPS51220 12V output is connected to the BATT pin of the BQ25713, simulating 3 cell battery. The problem occurs when the output of the BQ25713 transitions from 5V to 20V. There is a large amount of in rush current with consecutive current spikes follwoing, until the PPHV/VBUS rail eventually collapse. I am trying to determine what could be causing the PPHV/VBUS lines to collapse and if my implementation of the TPS51220 is at fault. When I use an external bench supply to replace the 12V supply from the TPS51220, the system works perfectly fine.
I also have a few questions that if you could answer would be helpful
- Why is there such a large voltage drop from the TPS51220 that never seems to recover? Shouldn't the feedback circuit of the TPS51220 kick in?
- What would cause the consecutive current spikes?
Using the TPS51220 to supply V_BATT
Using an external bench supply for V_BATT