Hi,
I have a question reading TLV1117 and P2P ON SEMI NCV1117, the current limit of TLV1117 is 1.2A, but the short-current VS (vin-vout) curve shows at vin-vout=5V, the short current is around 1.5A, which is conflict with the current limit parameter. Is this the parameter error or different test condition like different vin/vout?
And the short-current VS (vin-vout) curve shape of TLV1117 is different from NCV1117, is this because TLV1117 uses brick-wall current limiting while NCV1117 uses foldback current limiting? If yes, why TLV1117's short-circuit current show a increasing trend as the (vin-vout) increases? It shouldn't be decrease as the power consumption increases to easily reach OTP?
Best Regards,
Chen