I have a BQ24074 set to charge a 1.75Ah lithium battery at its recommended charge current of 875mA. When performing a battery charge test at 40C, it appears the fast charge portion of the cycle ends after about 32 minutes, and the measured battery voltage at that time is 4.02V. I am seeing very similar behavior when charging the battery at room temperature (~21C), where the voltage at which the charge begins to taper is 4.03V. Is this a curve of a device entering thermal regulation? Considering the input voltage is from a 5V USB power adapter, I find it hard to believe that a charge current of 60% of part's maximum designed current could be entering thermal regulation, especially after 30 minutes. Board has the appropriate layout with thermal pad and thermal vias, and is enclosed in a plastic housing with the battery. Should I see a constant current phase until I get into the Vbatreg range of 4.16-4.23V?
I'm thinking this is a normal charge curve, but would like a 2nd opinion from TI or other users of this device.
Entire charge curve:
Detail view: