Hi Good afternoon,
For the above mentioned part number LM76003, to obtain the dynamically programmable output voltage, from 6 to 24 volts, according the duty cycle of PWM signal, which is taken as input.
1. How can I make a setup at the input side, so as to receive a PWM signal of frequency 50 Hz , having a time period 1 us, and duty cycle from 5% to 10%.
2. How can I get a output voltage programmable according to the duty cycle of PWM signal received.
Please guide and do the helpful.
Thanking you in advance
Ramya.L