Other Parts Discussed in Thread: LM5176, LM5175, , LM5114, UCC27511A, CSD
Dear *,
i want to use CSD19534Q5A as low side output switch in buck-boost converter ( LM5176 CCM or LM5175 DCM).
a)
Do we need a mosfet driver between LM517X LDRV2 pin and the gate of the CSD19534Q5A mosfet ? ( max Fsw of LM517X is 500kHz)
b)
if the driver is not needed but will lower the switching losses, what is the right way to choose one regarding to driver driving current capability?
c)
what is the reasonable driver rise and file time (ns) to choose for CSD19534Q5A regarding to drive current , Fsw of the LM517X , Ciss 1000pF, Qg 17nC @ gs=10V and how it is calculated?
d)
how is the output voltage of the driver related to driver power supply ( Vcc) ? Vout= Vcc? So if Vgs needs 10V then set the VCC of driver to 10V?
e) we would like to choose newer driver IC regarding to cost defective solution.
Would you recommend one of the following IC LM5114 or UCC27511A?
Best Regards.