hi!The schematics design is like the AM335x starterkit's
when the IC is powered on, the voltage measured on this board:
VRTC=2.5
VCC1=5
VCC2=5
VCC3=5
VCCIO=5
VDIG1=5V
VDIG2=3.3
VAUX33=3.3
VAUX1=0.9
VAUX2=2.36
VMMC=3.8
VREF=0.85V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi!The schematics design is like the AM335x starterkit's
when the IC is powered on, the voltage measured on this board:
VRTC=2.5
VCC1=5
VCC2=5
VCC3=5
VCCIO=5
VDIG1=5V
VDIG2=3.3
VAUX33=3.3
VAUX1=0.9
VAUX2=2.36
VMMC=3.8
VREF=0.85V
Referring to this document:
TPS65910Ax User's Guide for AM335x Processors |
The following voltages should be present on the LDO output rails:
And the TPS65910 datasheet shows:
Please refer to the TPS65910 Schematic Checklist and see if there are any issues with the wiring of the TPS65910 that need to be addressed.
It is concerning that only one of your LDO outputs is producing the correct voltage. The internal bandgap voltage (VREF) is correct, but none of the other voltages are correct except for VAUX33.
You are using the TPS65910A3 version, which turns on VRTC in low-power mode. Have you tried using the TPS65910A31 version, which turns on VRTC in high-power mode? This is the only debug method I can recommend at this time.
Hi, 6238334,
Would you please let's know how many boards have the issue? It may be a cold soldering issue; I mean it looks like the device is not soldered properly.