Hi
i was trying to do a design that is based on a web bench tool results for a SEPIC. unfortunately when i try to implement the design in real life i keep damaging pin 9 of each LM3481 after a power cycle. at the moment it does not matter if i wait a long time for pin to discharge or not. attached is the schematic from the webbench tool and the one i have build up. any feedback would be helpfull.
Vinmin = 10V, Vinmax = 30V, Vout = 24.5V, Ioutmax = 1.0A
there is a 10uF bulk at input not shown in the design.