Design requirements: VCC_ When 5V is not working, the lmz31710 does not output voltage. When VCC_ After the 5V voltage is started, the lmz31710 outputs 1v0 voltage. The lmz31710 has no en, and the INH pin is used to control the chip start.
Questions:
1. Can functional requirements be realized by MOS switch as follows?
2. It is mentioned in the manual that INH pin has built-in pull-up resistance, but the resistance value and pull-up level are not mentioned. How to determine the external pull-down resistance value?
3. Please help to see if the schematic design is reasonable?