Hi Peter,
following the question of that half bridge power supply, the operation conditions is as below:
Switching frequency:100 kHZ
Input voltage: 200~800 Vdc
Output voltage: 24 Vdc
Output power: 180W Rated,216W Max,
XFMR turn ratio: 3.714,
Primary inductance:1000uH typical,
Input voltage feedward used, voltage mode,
Primary side control,
use diodes as secondary side rectifier,
Type III compensation network with TL431B and Zener.
Since I use the input voltage feedward function, I put 813kohm resistor and 470pf cap on the pin RAMP/CS, when the input voltage exceeds 400V, the voltage at pin RAMP/CS is clamped at 4.3V, the higher input voltage, the higher slew rate of RAMP/CS.
what is the consequence of clamping the voltage at 4.3V continuously? So far, I didn't see any failure related to this, since I have done the HALT test, thermal cycling and high temp acceleration test on so many samples.
if i still want to use this input feedward function, what is the recommended value of Rramp (considering 200V~800V input) to keep RAMP/CS voltage below 4.3V?
if i don't use input feedward function, what is the recommended value of Rramp and Cramp when connecting to Vref?
Best regards,
Chengjun