Hi Team,
For Table 6 -1 Power Sources in the datasheet,
The rated output current is VBAT intended for 3.6 V or 5 V?
Thanks,
Taishi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
For Table 6 -1 Power Sources in the datasheet,
The rated output current is VBAT intended for 3.6 V or 5 V?
Thanks,
Taishi
Hi,
Looking at the BOOST/VDD3 output voltage of 5V, i think that VBAT is set to 3.6V. But in general, other BUCK regulators and LDO's should be able to support 5V VBAT as well, but there may be limitations related to device temperature/thermal performance. I have forwarded your request to this device expert and he will provide you the confirmation.
Regards,
Murthy
Hi, Taishi,
As long as the dropout voltage between VBAT and VOUT is met, the rated output current is applied if device is still working in the temp specified by datasheet.