Hey all,
Using this device, I know I can control the charging of the battery using the CE pin or REG01(5:4) bits but is there also a way
to force the device to power SYS only from the battery, even when a valid charger is powering the VBUS input?
Also, how 'healthy' is it for a lit-ion battery if I connect a load to SYS which is changing from zero to about 2 amps in cycles of a few seconds all while VBUS is connected and trying to charge the battery
at the same time (1A charge current), assuming VBUS can handle this load?
Thank you!
Nir