Hello, If I use more than one DCDC Converters and MCUs, then which is right way to split ground?
For example, I am going to use three LMR33630, and each LMR33630 gives power to each MCU.
LMR33630 or any other dcdc converters also have PGND and AGND each.
If I use One DCDC and One MCU, then I will connect DCDC's AGND with MCU's AGND and then connect whole PGND and AGND with 0Ohm.
But If I use more then one, and if each devices's are too far from each other then how to split agnd?
Split each agnd and connect each 0Ohm to pgnd plane?
or connect agnds all together with narrow lines and use only 0 ohm to pgnd plane?
Which is better? Or is this wrong?
Thanks.