Hi,
I'm trying to understand why, during simulation with TINA, a TPS61169 oscillates in and out of discontinuous mode at about 60kHz (see SW_V, the voltage at the switch pin 1, below). My input filter impedance peaks at 1.5 ohms at 10kHz. I've tweaked every component that could affect the TPS61169's control loop response to no avail. Inductor is 10uH; input and output caps are 4.7uF. Can it not stay in continuous mode while driving eight sets of three white LED strings (8.3V @ 135mA) from a 5V supply?
Fred