Other Parts Discussed in Thread: INA233,
Hello,
I always receive 0xFF bytes from the device. No matter what the read function is. I tried with MFR_ID (99h), READ_VIN(88h), READ_VOUT(8Bh) and READ_TEMPERATURE(8Dh).
The device answers me with acknowledges but data(s) is(are) FF in all the cases.
The analog part of the device seems to work normally.
Here after are two captures of the communication I have with the board for 88h and 8Bh functions. I assume I miss something because I changed the device and the problem still remains.
Note that SDAI and SDAO are connected on my board.
Thanks in advance for you help,
Maxime Javaux