Hi
We have contacted you to confirm the specifications of the Charger IC "BQ25600D". Please kindly answer the following questions.
1. About switching efficiency
Regarding the efficiency of the charging IC, we have confirmed the specifications below.
We set 960mA charging, could you provide us with numerical values for min, typ, and max values for efficiency in that case?
If you need the calculation and the conditions, please let us know.
2. About VBUS current
It is related to the first check item.
Is it possible to calculate the min/max VBUS current below following conditions in order to confirm?
- VBUS voltage range: 4.8V to 5.2V
- VBAT voltage range: 3.7V to 4.0V
- Charging current: 960mA
- SYS side: No load assumption (about 30uA)
If you need additional conditions, please let us know.
We apologize for the inconvenience, and thank you for your cooperation.
Best Regards,
FUKUYA