Hi Texas Instruments Customer Support
Thank you for your support, I have some questions for TPS546D24A, thanks.
Please see the attached file. Thanks
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Texas Instruments Customer Support
Thank you for your support, I have some questions for TPS546D24A, thanks.
Please see the attached file. Thanks
Regards
In the future, please post questions directly into the text of the E2E post rather than attaching them in files. Post text is searchable to help other people with similar issues find your question and our answers, text in attachments is not searchable.
If I want to select Address(0x10h(16d)), I will set resistor to AGND (Code 0), but divider code have a lot of (16-31),
How can I set it? thanks.
The ADRSEL to BP1V5 resistor selects the SYNC to internal oscillator phase shift, and the direction of the SYNC pin's function. You will want to select it depending what you want to do with the SYNC pin.
Condition (1Phase power)?
SYNC is available, but not required on 1-phase or "Stand Alone" power where a single device provides the output.
Condition (2Phase power)?
Hi Texas Instruments Customer Support
Thank you for your support,could you help me?
I have new questions for TPS546D24A, thanks.
Please see the attached file. Thanks
Regards
Richard
Please include your questions in the text of your response and not in an attachment, which does not allow for searching. If you wish to copy from Microsoft Word, you can use the "Paste from Word" button in the reply tools bar
Thank you for your support, I have some questions for TPS546D24A address, thanks.
V01~V05 is 1Phase power.
If I will set FPGA to control the V01 V02 V03 V04 V05 on the same PMBUS.
Address condition
V01=0x11h (17d)
V02=0x21h (33d)
V03=0x15h (21d)
V04=0x25h (21d)
V05=0x48h (72d)
Could you help me?
How can I set it? thanks.
The TPS546D24A PMBus Address is programmed through the ADRSEL pin (Pin 31) with a combination of the resistor to ground and the resistor divider. The relevant chart is table 15.
V01=0x11h (17d) Select Resistor to AGND code 1 with an EVEN (0,2,4..14) divider code
V02=0x21h (33d) Select Resistor to AGND code 1 (same resistor as above), with an ODD (1,3,5..15) divider code
V03=0x15h (21d) Select Resistor to AGND code 5 with an EVEN divider code
V04=0x25h (21d 37d) Select Resistor to AGND code 5 with an ODD divider code
V05=0x48h (72d) Select Resistor to AGND code 8 with an ODD divider code.
Resistor to Ground resistor for code 1 and 5, along with the divider codes, are given in table 17 while code 8 is given in table 18.
For Resistor to Ground code 1, the Pin to AGND resistor is 5.62kOhms (circled in red)
For Resistor to Ground code 5, the Pin to AGND resistor is 12.1kOhms (circled in blue)
The Pin to BP1V5 resistors to select EVEN divider codes with 5.62kOhms in table 17 are circled in green. Which resistor you want to select depends on how you want the SYNC pin configured.
The resistor for pin to ground code 8 is 21.5k (circled in red) and the resistor to BP1V5 for ODD divider codes are circled in green.
Assuming you want to synchronize all of the devices to a common clock to reduce input voltage noise, select one of the VR devices to be SYNC_OUT, I will use your V01
The Even divider code for SYNC_OUT with 0 phase position is code 12, so the ADRSEL pin of V01 would have 5.62kOhms to AGND and 1.54kOhms to BP1V5
Now, selecting SYNC_IN for the other rails, the ADRSEL to BP1V5 resistors would be:
V02: SYNC_IN, 90 Degrees, Divider Code 3 under 5.62kOhms : 11.0kOhms
V03: SYNC_IN, 120 Degrees, Divider Code 4 under 12.1kOhms: 18.7kOhms
V04: SYNC_IN, 180 Degrees, Divider Code 7 under 12.1kOhms: 10.0kOhms
V05: SYNC_IN, 270 Degrees, Divider Code 11 under 21.5kOhms: 7.50kOhms
There is also a useful tool available - http://www.ti.com/lit/zip/SLUC686 which allows you to select the desired address and SYNC configurations through drop-down menus, and it calculated the required resistor values.